What Pelco Protocols are supported by the MPT9500 keyboard controller?

Issue

MPT9500 supported protocols for PTZ control.

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • MPT9500 Keyboard

Cause

Supported protocol types for ptz control

Resolution

The MPT9500 Keyboard supports the following protocols:

  • STD COAXITRON (15-bit)
  • EXT COAXITRON (32-bit)
  • PELCO D 2400     (RS-485)

Click here to view the I/O manual.