KBD300A With 12VDC transformer

Issue

Use a 12VDC transformer on the KBDKIT to power up a KBD300A

Product Line

Pelco Matrix

Environment

  • KBD300A
  • KBD4000
  • KBD200A
  • KBDKIT
  • Power supply
    • 12 VAC .20A
    • 12 VDC .20A

Cause

Installation with 12VDC

Resolution

It is possible to use a 12VDC transformer on the KBDKIT wall block to power the KBD series

  • Pin 3 is DC (+) Positive connection.
  • Pin 4 is DC (-)  Negative connection

 

 

Note: RJ-45 Port PIN Out without using the Wall Block: (W/B) PIN 7 = RX-, (B)PIN 8 = RX+ connect to TX- and TX+ on the Controller and PIN 5 and PIN 6 (B/WB) = 12 VAC/DC Non Polarity