Getting Office Outlook default mail client error message on startup of Continuum.

Issue

Continuum presents an error when starting up.

"Either there is no default mail client or the current mail client cannot fulfill the messaging request. Please run Microsoft Outlook and set it as the default mail client"

Product Line

Andover Continuum

Environment

Continuum Cyberstation

Microsoft Outlook

Cause

When Outlook is installed on the Workstation, Continuum will try to make a connection to Outlook when it starts up. If Outlook has not been configured as the default mail client then it can't make this connection and presents the error.

Resolution

Either make Outlook the default email client or uninstall from the Workstation. See Microsoft KB here that describes how to set your default email client.