Replacement to the EA2000 or the EA2000/220 devices.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

  • I hear that the EA2000's are becoming obsolete; what can I replace them with?
  • What is the replacement model to the EA2000?
  • What I can use in place of the now obsolete EA2000?
  • What is Pelco providing to do the same thing as the EA2000?

Product Line

Pelco Transmission & Power

Environment

  • EA2000
  • EA2000/220
  • EA2010

Cause

The EA2000 is obsolete

Resolution

  • There is no current product offered that will take the place of the EA2000 nor the EA2000/220.
  • The EA2010 is NOT a valid replacement as the EA2010 is Video Only and will NOT pass Coaxitron like the EA2000 devices will.