Issue
Can a soft or hard reboot command be sent to a MNB controller from a Niagara R2 UNC-520?
Environment
Niagara R2
Cause
Avoid the need for using the WorkPlace Commissioning Tool
Resolution
Any kind of reboot command from a Niagara R2 station, to a MNB controller, is not possible.
The WorkPlace Commissioning Tool is required.