Issue
Which Modbus driver is required for I/A Series Niagara G3 ENC-520 to support Modbus TCP?
Environment
I/A Series G3 ENC-520, JACE-645, JACE-6E, JACE-7, JACE-NXT, ENC-SW
Cause
Select the correct part number to enable the ENC to function as a Modbus TCP Client (Master) or Server (Slave).
Resolution
ENC-DRV-MOD-T (ENC 520 acts as Modbus master (client) using Ethernet TCP)
ENC-DRV-MOD-R (ENC 520 acts as Modbus server (slave) using Ethernet TCP)