Is DS ControlPoint compatible with Microsoft Windows 8 or 10?

Issue

Will DS ControlPoint install and run on a Windows 8 or 10 platform?

Product Line

Pelco Video Management

Environment

  • DS ControlPoint Client software versions
  • Microsoft Windows 8 32bit/64bit
  • Microsoft Windows 8.1
  • Microsoft Windows 10

Cause

  • Software update release DS ControlPoint version 7.6 is now compatible with Microsoft Windows 8 platform. This includes the Windows 8.1 update.
  • DS ControlPoint is now supported on Windows 10.

Resolution

DS ControlPoint v7.6.32 or later is compatible with Microsoft Windows 8/8.1 platform (x86 and x64).

Note: Windows 8 RT is ARM based technology which is primarily used on tablets and is not supported.

DS ControlPoint v7.15.70 or later is compatible with Microsoft Windows 10 platform.


Related Articles:
Where can I download the latest version of DS ControlPoint client software?