Where can I download the DX Series Export Viewer?

Issue

Where can I download the DX Series Export Viewer?

Product Line

Pelco Video Management

Environment

  • DX4500/DX4600
  • DX4700/DX4800
  • DX Series Client
  • Export Viewer
    • exp
    • avi

Cause

Export viewer to play back video exported from server.

Resolution

The DX Series Export Viewer is installed as part of the DX Series Client package.

The DX Series export viewer allows you to play back video that is exported from the server or the DX Series Client native format. You can verify the digital watermark embedded in native video. Watermarking is used to authenticate the originality of a video filed and to alert users to possible image tampering.

  • Click Here to download the DX Series Export Viewer software
  • Click Here to view the manual for DX Series Export Viewer.
  • See LL#12114 for downloading DX Series Client Software.

Note: The DX Series Client does not support the DX8100 Native format.

Related Articles:
How to review exported video (.exp) using the DX Series Export Viewer.