Issue
- Can I expand my DX4800 DVR like the DX8100?
- Is the DX8100-EXP compatible with the DX4700/DX4800 series DVR's?
- Can I expand my DX4700/DX4800 with the DX8100-EXP?
Product Line
Pelco Video Management
Environment
- DX4700 - all versions and all models
- DX4800 - all versions and all models
- DX8100 - all versions and all models
Cause
The DX4700/DX4800 series DVR's are NOT compatible with the DX8100-EXP nor can the DX4700/DX4800 series DVR's be expanded past the purchased chassis option (I.E. - 8 channel versus 16 channel)
Resolution
The DX4700/DX4800 series DVR's cannot be expanded to anything other than the model purchased. The DX8100-EXP is NOT compatible with the DX4700/DX4800 series products either.