Issue
Both errors indicate WorkPlace Tech cannot determine if the vsd file being opened is in the current project.
Environment
WorkPlace Tech
Cause
The names of the folders that were brought forward contained an apostrophe, i.e. Vav's, AHU's, etc.
Resolution
Rename the folders eliminating the apostrophe before bringing the folders\drawings into the new project and these errors will not occur.