How can arrays be used when programming Continuum controllers using StruxureWare Building Operation?

Issue

Unable to migrate programming over from Continuum as program use Numerics configured as global arrays. How can arrays be used in StruxureWare Building Operation?

Product Line

SmartStruxure Solution

Environment

Enterprise Server

Automation Server

b3xxx

Cause

Under StruxureWare Building Operation, objects can no longer be setup as global arrays using manual log entries.

Resolution

You are still able to use local arrays in Programs and Functions. Modify your Pain English program code so that they use local arrays (defined within the Program or Function) rather than global arrays (defined in the numeric/input as a manual log).