Issue
SNVT bindings to the LNS Network Interface do not update when viewed in Vista
Environment
Vista 5
Lonmaker 3.2
NL220
Cause
When a binding to a dynamic SNVT in the LNS Network Interface is created or modified, there is no indication in the System Plugin that an update to the Vista database is required. However, if the Vista database is not updated, newly created dynamic SNVTs will not appear in the $Host folder in Vista and existing, modified bindings will stop updating.
Resolution
Ensure that the Vista database is updated from the System Plugin after every change affecting bindings to the LNS Network Interface.