Issue
V298 is obsolete and needs a replacement
Environment
V231:
7213106000
7213110000
7213114000
7213118000
7213122000
7213126000
7213130000
7213134000
7213138000
7213142000
7213146000
7213150000
V298:
7219818000
7219822000
7219826000
7219830000
7219834000
7219838000
7219442000
7219846000
Cause
Obsolete valve needs replacement
Resolution
V298 valves can be replaced by valves from the V231 family. For more details, please see the data sheets for each valve model.
Please note that the V298 closes with stem down, while V231 closes with the stem up.