Issue
When an Access Event is received at the CyberStation from a controller under a network on a different time zone, will the time shown be that of the CyberStation receiving the event or the time stamp from the remote time zone?
Environment
CyberStation
Cause
Documentation
Resolution
Access events show the time stamp from the zone where the controller is located.
So if an Access Event is received at a CyberStation located in (GMT-05:00) Eastern Time from a controller located under a network in the (GMT-08:00) Pacific Time the time stamp shown by the event will be Pacific time.