FD5-IRV10-6 camera image is a Pink or yellow Hue color.

Issue

FD5-IRV10-6 displays pink or yellow tint in color.

Product Line

Pelco Cameras

Environment

  • FD5-IRV10-6

Cause

Video image is displaying pink in color

Resolution

The lighting type environment may require some adjustments to the camera settings for true scene color. Adjust the following settings for color scene adjustment:

  • If camera is being installed outdoors, change default programming of camera from INDOOR to OUTDOOR setting.
  • Change White Balance to environment color temperature if required. (view image here for menu section from I/O Manual)