Esprit ES30C/ES31C-2N System with single Illuminar IR623-P Series Illuminator

Issue

Esprit with single IR Illuminator

Product Line

Pelco Cameras

Environment

  • ES30C-2N/3S31C-2N (24VAC) Models
  • SMR1-1NQG2D
  • IR623-P Series

Cause

Single Illuminator with Esprit

Resolution

To request the Esprit ES30C/ES31-2N with Pre-installed Brackets to support single Illuminar IR623-P Series Illuminator.


From Pelco Dealer:

  • Select 24VAC Esprit Model.
  • At time of Esprit order request SMR1-1NQG2D
  • Installation Guide view.

SMR1-1NQG2D: Designed to integrate a single IR623-P Series Infrared Illuminator that follows the positioning and full 360 rotation of the Esprit Series camera. SMR is to add mounting bracket to Esprit.

  • Click Here for Bracket Explosion view. IR lamp illustrated as reference only and is not supplied by Pelco.

From Illuminar Inc:

  • Request IR623-P Series. Click Here to view Specification Sheet to IR623-P Series and additional information.