Plain English Function does not work.

Issue

When the sample code supplied under Continuum Help for the Select Case function is pasted directly into a program a controller the function does not work.

Continuum generates the following error.  "Process not supported"

Product Line

Andover Continuum

Environment

  • Plain English functions
  • Select Case

Cause

Some PE functions are supported in specific Continuum products only.

For example, Select Case is supported only in CyberStation.

Resolution

Check the Products Supported section of the Continuum Help on Select Case functions. 

Select case is supported in CyberStation only.