What international standards and approvals has SmartStruxure been tested against?

Issue

What are the product certifications?

Product Line

SmartStruxure Solution

Environment

SmartStruxure for Buildings

AS, ES

Cause

Standards documentation required.

Resolution

Click here for the CE Declaration of Conformity

Click Here for the WSPCert

For  BACnet BTL Testing see the PICs statements or the BTL Website:

http://www.bacnetinternational.net/btl/

For UL and Country of Origin certification, please refer to PSS for this.