Duplicate Cardholder when using the PIU (Personnel Import Utility)

Issue

After using the PIU there are duplicate cardholders

Product Line

Andover Continuum

Environment

Continuum

PIU

Windows XP

Windows 7

Windows Server 2003

Windows Server 2008

Cause

A unique alias must be specified with the transform or duplicate records will be created

Resolution

Each alias must be unique. Information that is updated for a personnel object will be triggered off the alias. If the alias already exists in the database, then just the new information is added. If the aliases are not unique, a new record will be created. (See “Saving a Configuration and Importing Data into CyberStation.”) To verify this, when previewing your data, make sure that every alias name under the "Alias" column is unique before importing.

See Lessons Learned Article #13732 for more information