Esprit Series PTZ (Pan, Tilt, Zoom) must be level when mounted.

Issue

The gear assemblies in the Esprit Pan Tilt module will slip and the enclosure will drift on it's Pan axis if the unit is not level.

Product Line

Pelco Cameras

Environment

  • All Esprit Series - all model all versions.

Cause

  • Installation and service

Resolution

Be sure to mount the esprit so that the end result is a flush, plum, and level installation.