Guard Tour for I/NET

Issue

Guard Tour for I/NET

Product Line

TAC I/NET

Environment

I/NET site with Access Control

Cause

Is there a Guard Tour configuration or is there add-on software for Guard Tour with I/NET Access Control

Resolution

I/NET really does not have a Guard Tour add-on. It does not have a Guard Tour setting with the Access Control functionality. 
 
What I would suggest however, is that you can run a report on an individual card, and this report could have the times at which the card was used. This could for example be the Guard card, and show that at specific times the Guard used the card. This also would apply to a Group such as Guards.
I/NET does not have a Guard Tour add-on. It does not have a Guard Tour setting with the Access Control functionality.
 
However, a site can run a report on an individual card(s), and this report could have the times at which the card was used. This could for example be the Guard card, and show that at specific times the Guard used the card. This also would apply to a Group such as Guards.
 
Please find two custom reports for using with the above suggested scenario. 
Custom Reports.zip which contains two reports:
  • TAC_TransactionsIndividuals_dateIndivID_001.rpt
  • TAC_TransIndiv_Date_IndivID_GroupName.rpt