Restart the DX8000/DX8100

Issue

How to restart the DX8000/DX8100 series

Product Line

Pelco Video Management

Environment

  • DX8000 Series
  • DX8100 Series

Cause

Rebooting DX8000/DX8100

Resolution

To Reboot the DX8000/DX8100 graphical user interface System, perform the following:
 
1. Log into the DX8000/DX8100 graphical user interface using the appropriate default credentials:
 
Default credentials for DX8000/DX8100 HVR version 1.2 and lower:
Username: Admin
Password: Admin

Default credentials for DX8100 HVR version 2.0 and higher:
Username: admin
Password: admin
 
2. From the DX8000/DX8100 menu bar, choose File > Exit. The Shut Down dialog box opens.
3. From the Drop-down menu, select "Restart" and click "OK". Once the DX8100 GUI has shut down, the DX8000/DX8100 will then reboot.
 
Note: Usernames and passwords are case-sensitive.