Web Page adjustment of Sarix Resolution settings do not save.

Issue

When I adjust the IE30DN resolution settings, the IE30DN always defaults to previous settings.

Product Line

Pelco Cameras

Environment

  • Sarix IP cameras
  • Digital Sentry
  • IE Web Page

Cause

Adjusting resolution settings through IE Web Page for higher or lower value does not save

Resolution

When an IP camera (Sarix) is linked to the Digital Sentry system, edit of resolution for Sarix must be done from the DS system and not from the Sarix web page. Sarix web page will not hold settings due to stream being requested by DS.

View LL#10387 for adding or editing IP camera settings through DS