Deleting the Array on a DX9200HDDI.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Instruction how to delete array on a DX9200HDDI.

Unable to configure the DX9200HDDI for RAID5.

Product Line

Pelco Video Management

Environment

  • DX9200HDDI
  • DX8100 Series
  • DX9000 series

Cause

  • Damage Array on DX9200HDDI

Resolution

Delete array's on DX9200HDDI:

  1. On the DX9200HDDI control panel,Press the CTRL button. The TO CONTROLLER PRESS ANY KEY message is display on the LCD screen.
  2. Press the check mark button. The Enter Password prompt is displayed.
  3. Press the check mark button to enter 00000000 (default password).
  4. Press the check mark button The Main menu is displayed.
  5. Select array 1, From the Main menu, press the up/down arrow button to display (2) RAID Params.
  6. Press the check mark button. The (2) RAID Params menu is displayed.
  7. Press the up/down arrow button to scroll to (21) Array 1.
  8. Press the check mark button.The (21) Array 1 menu is displayed.
  9. Press the up/down arrow button to scroll to (211) Re-Conf RAID.
  10. Press the check mark button.The (211) Re-Conf RAID menu is displayed.
  11. Press the up/down arrow button to scroll to YES.
  12. From the (21) Array 1 menu, press the up/down arrow button to scroll to (212) RAID Level.
  13. Press the check mark button.The (212) RAID Level menu is displayed.
  14. Press the up/down arrow button to scroll to NONE.
  15. Delete Array 2, Press Exit to (2) RAID Params menu is displayed.
  16. Press the up/down arrow button to scroll to (22) Array 2.
  17. Press the check mark button.The (22) Array 2 menu is displayed.
  18. Press the up/down arrow button to scroll to (221) Re-Conf RAID
  19. Press the check mark button.The (221) Re-Conf RAID menu is displayed.
  20. Press the up/down arrow button  to scroll to YES.
  21. From the (22) Array 2 menu, press the up/down arrow button to scroll to (222) RAID Level.. 
  22. Press the check mark button.The (222) RAID Level menu is displayed.
  23. Press the up/down arrow button to scroll to NONE
  24. Exit out to Main Menu.
  25. Press the up/down arrow button select NVRAM.
  26. Press the up/down arrow button select "Update NVRAM"
  27. Press the up/down arrow button select "Restart"
  28. Confirm the DX9200HDDI Front panel LCD display show all "S" for each hard drive install and "X" if no harddrive.