Automation Server Lonmark Certification

Issue

Does the Automation server have Lonmark Certification  

Product Line

SmartStruxure Solution

Environment

Automation Server

Cause

Specification requirement is for Lonmark certified devices

Resolution

There are no current plans for this.The reason is there is no suitable profile.

LonMark have been working on a profile for these types of devices over many years now, and their is no information on  if/when this will be approved. 

The AS is design and developed to behave like a LonMark certified device, but it contains no application which all existing profiles requires.