The Station buttons are missing in the MCU Configuration dialog box

Issue

The Station buttons are missing in the MCU Configuration dialog box

Product Line

TAC I/NET

Environment

I/NET 2000 Site

Cause

The Station buttons are missing in the MCU Configuration dialog box. What happened?

Resolution

To provide you with the ability to configure or hide the statistical features of I/NET 2000, there are three .reg files included in the I/NET 2000 application root directory. When you double-click the desired *.reg file, it will update the DiagnosticFlag in the registry to the associated condition.

Each file and its function is as follows:

  • NoStats.reg - No statistics dialog shown,
  • Stats.reg - Shows statistical data but does not allow back-ground ASC resets or manual MR/ASC resets,
  • Stats&Reset.reg - Shows statistical data with ability to perform background ASC resets or manual MR/ASC resets. 

For more information see TCON 217.