Issue
Unable to connect to b3xxx controllers with RoamIO.
Environment
RoamIO-1
RoamIO-2
Cause
The RoamIO-1 is not able to communicate with BACnet controllers. It only supports Infinet controllers.
Resolution
The RoamIO will not be able to communicate with the BACnet controllers (bCX4040, b3xxx, etc...) you will need to use the RoamIO-2 that is able to communicate to both Infinet and BACnet.