What DX8100 software version can be installed on the DX8100 server?

Issue

Don't know which DX8100 version software can be installed.

Product Line

Pelco Video Management

Environment

DX8100 Series

Cause

There are different DX8100 versions.

Resolution

  1. Confirm which operating system is running on the DX8100 server.
  2. Reboot DX8100 server and during boot up you will see Windows2000 or WindowsXP splash screen.
  3. Download DX8100 server software.
  4. Created a bootable disk. refer to article LL#8830

More information on how to run recovery software on DX8100 refer to article LL#10571