Issue
Requests for information on a wireless access control solution
Environment
Continuum
Schlage
Windows XP
Windows 7
Windows Server 2003
Windows Server 2008
Cause
Easy access to documentation for the Schlage Wireless Access Control Solution
Resolution
09-17-2012 The Security Center of Excellence is pleased to announce the integration between Schlage AD-Series locks and Andover Continuum Netcontroller II and ACX 57XX family of controllers. This integration will provide a cost effective and scalable access control solution. Schlage AD-Series locks combine all of the components typically found around the door such as the door position switch and the request to exit switch into one unit which simplifies installation and saves money. Since they are designed to be modular Schlage AD-Series locks can easily be upgraded in the future to meet changing security and technology requirements. Within Continuum Cyberstation the Schlage locking device will look and function like a normal door and an XDriver at the controller level will provide access to these devices. This solution is ideal for education and healthcare facilities but can also be used in a wide range of other applications. For more information please contact COE@Buildings.Schneider-Electric.com.