Time schedules and special day are not working correctly

Issue

time schedules and special day are not working correctly

Product Line

TAC I/NET

Environment

I/NET Site

Cause

Time schedules and special day are not working correctly

Resolution

If the regional settings in windows (inside the control panel) are not set correctly these schedules will not function correctly. The settings need to be as follows: The short date style mm.dd.yyyy The long date style mmmm.dd.yyyy