Spectra IV outdoor model heater connection

Issue

How is the heater connected to door assembly

Product Line

Pelco Cameras

Environment

  • Spectra IV Outdoor
  • BB4-PG-E
  • SD435-PG-E0

Cause

View of internal wiring connection for heater to door assembly

Resolution

The outdoor Spectra IV provides internal heater wiring connection that requires no user adjustments or additional wiring.

Here is a view of how the heater connects from the side panel assembly to the BB4DOORASSY.



 Note: The housing and camera receive power from the same input power source and no additional cabling is required for heaters.