Integration to CAN bus protocol

Issue

Integration to CAN bus protocol

Product Line

TAC I/A Series

Environment

I/A Series R2
I/A Series G3

Cause

There is a need to integrate to devices where the available communications protocol is CAN bus. 

Resolution

I/A Series does not have a driver for CAN bus protocol. A third party converter / gateway can be used to convert CAN bus to a standard protocol available in I/A Series. 


The following company was found after a search on the Internet. They offer solution for CAN bus to various communications protocols.

http://www.adfweb.com/home/default.asp

http://www.adfweb.com/home/about/about.asp

 

Note: Please note Schneider Electric do not endorse this product but provide this option as a workable solution. All support issues related to these products should be sent directly to their support centers.