Issue
Does the oBIX service in I/A Series R2 require the web services license feature to operate?
Environment
I/A Series R2, UNC, oBIX
Cause
Licensing requirements for I/A Series oBIX
Resolution
The web services and associated license feature (webUi) is not required to run the oBIX service in an I/A Series R2 station. The feature line in the R2 license must include obix.
- UNC example ... features=coreRuntime;bacnet;lonworks;obix
If the license does not include the obix feature, purchase part number IA-DRV-OBIX for each Enterprise Server / UNC that needs to function as an oBIX server.