Converting I/NET Symbol Libraries to TGML Components

Issue

Converting I/NET Symbol Libraries to TGML Components

Product Line

TAC I/NET, SmartStruxure Solution

Environment

I/NET TGML Graphics Converter

Cause

Many users want to continue using the same graphic libraries they had in I/NET while in StruxureWare. The TGML conversion tool, will convert these libraries to TGML components.

Resolution

  1. From Either I/NET or StruxureWare Workstation, open the I/NET graphics Conversion tool
  2. Select the Symbols check box on the right hand column
  3. Browse to the source and destination folders
  4. Select the files you wish to convert.
  5. Click Convert
  6. In Windows Explorer Browse to the destination folder.
  7. You can double click on each component to automatically add it to your "My Components" Component Library. NOTE: Be sure the TGML Editor is closed while you do this.
  8. Once you have finished this, open the TGML Editor and note that your My Components Library is now full.
  9. If desired, you can change the name of this library for sorting purposes or future exporting.