Illegal object name characters in StruxureWare Building Operation

Issue

What constraints must be followed when naming objects in StruxureWare Building Operation?

Product Line

SmartStruxure Solution

Environment

  • Building Operation Workstation
  • Object naming
  • Illegal characters

Cause

Using incorrect object names can may cause unpredictable results in SmartStruxure.

Resolution

Refer to WebHelp article #6429


All objects in the StruxureWare database have to have a name. StruxureWare is case-sensitive and differentiates between upper and lowercase characters.

Two objects cannot be named in the same way in the same folder even if the objects are of different types. For example, you cannot create an alarm named Building A and a graphic named Building A in the same folder. However, if you name the graphic Building a, with a lowercase a, you can create it in the same folder as the alarm object Building A.

The following characters are not allowed in object names in StruxureWare Building Operation.

         

  • /
  • "
  • ?
  • *
  • ~
  • &
  • White space is not allowed in the beginning or the end of an objects name.
  • . (period) is not allowed in the beginning of an objects name.
  • There is no limitation of how many characters an object name can have.

 

NOTE: If an apostrophe (') is used in the Enterprise Server name, Webstation will have some issues with page links. Here is a link to this issue.