Analog ExSite wire cable connections

DANGER

HAZARD OF ELECTRIC SHOCK.
Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.

Issue

Wiring assignment for IPSXM-2 or IPSXM-7 power module

Product Line

Pelco Cameras

Environment

  • ExSite
  • EHXM Fixed Explosion proof
  • IPSXM-2
  • IPSXM-7

Cause

Wiring assignment of base transformer

Resolution

 

WARNINGS:

  • Be sure to seal the cable entry conduit fitting with the appropriate sealant (not supplied) during installation.
  • When installing this unit, provide access to the communication wires (TX- and TX+) to allow connection to the system for future software
    upgrades. Connectors must be installed so that the integrity of the hazardous location is maintained. These communication wires are
    required even if the system uses coaxitron control. Maximum wire distance for RS-422 data wires is 1,219 m (4,000 ft).



Click here for Label Pin out
Click here for EXAC view

NOTES:

  • Relay 3 is allocated specifically for an external washer (not supplied by Pelco)
  • All relays are specified for 32 VDC, 0.5 A.
  • Wiring/cable for UTP and fiber optic are not provided on the wire harness. The installer must provide UTP and fiber optic connections