How do I install the In Ceiling Spectra series back box?

Issue

Spectra back box in-ceiling installation

Product Line

Pelco Cameras

Environment

  • BB5-F
  • BB5A-F
  • BB53-F
  • BB4-F

Cause

Installation of housing within ceiling

Resolution

The following tools are recommended for installation of the Spectra series in-ceiling housing:

  • Pencil
  • Drill with 3/32-inch drill bit.
  • Compass Tool (provided. view image here)
  • Mini Hacksaw
  • Phillips Screwdriver

 

HARD CEILING INSTALLATION - PREPARE CEILING:

  • Locate the center point of the mounting location. Drill a hole in the ceiling using a 3/32-inch drill. Insert the compass into the hole. Use a pencil and the compass tool to draw a circle on the ceiling. Carefully cut out the circle.

  • Refer to the linked manual for housing installation details. Click here : C2441M (2/02).
  • View housing dimensions here.