What is required to upgrade a UNC 196 outstation to a Sigma x96 controller?

Issue

Upgrading a UNC 196 outstation.

Product Line

Satchwell Sigma, Other

Environment

UNC

196

296

Upgrade

Cause

Customer wishes to upgrade his BAS outstation to a Sigma controller.

Resolution

To upgrade the outstation the following cards will need to be replaced.

Comms/CPU Card

Power Supply Card.

These can be purchased together as an S-x96-UPKIT

If the outstation also contains a Maximum Demand card, this is replaced by a Digital Input card (S-UNC-DI).