Reference changer not updating changes in OGC Graphic links

Issue

When the need arises to change object paths in OGC graphics the Vista reference changer does not work.

Product Line

TAC Vista

Environment

Vista 5.x.x

Cause

For unknown reasons the reference changer does not seem to work well on all OGC databases.

Resolution

The first thing to try is to edit the OGC after an attempt has been made with the reference changer.

If the links have been updated saving the OGC back to the Vista database can sometimes work.

If this did not work you can use the reference changer in the OGC editor.

Here is a link on that process.