KBD300USBKIT RS-422/485 USB ULINX is not compatible with the DX4500 DX4600.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

KBD300A not communicating with the DX45/4600 DVR recorder.

Product Line

Pelco Video Management

Environment

  • DX45/4600 DVR recorder V 1.4..6.
  • KBD300USBKIT (RS-422/485 USB ULINX) not compatible.
  • Belkin Model F5U409V1 USB to Serial (Customer Supplied)
  • PV140
  • KBD300A

Cause

  • The KBD300USBKIT new components are not communicating to DX45/DX4600 DVR. 
  • The Kit provides the PV140 RS-232/RS-485 converter, but the customer MUST supply the USB to Serial cable.
  •  Belkin Model F5U409V1 (Customer Supplied cable) 

Resolution

It is recommended to use the KBD300A with older KBD300USBKIT to communicate to the DX45/4600 DVR recorder.

View article LL#10342  for wiring older KBD300USBKIT to DX45/4600.

Note:
The new KBD300USBKIT (RS-422/485 USB ULINX adapter) is recommended for KBD300A and DSSRV installation.
The new KBD300USBKIT (RS-422/485 USB ULINX adapter) is recommended for KBD300A and DX47/4800(HD).
Images of old and new adapter view here.