Associate audio on the DX4100 Series Digital Video Recorder to a selected channel.

Issue

Cannot associate audio on the DX4104 Series Digital Video Recorder to a selected channel.

Product Line

Pelco Video Management

Environment

  • DX4104 Series Digital Video Recorder

Cause

Audio input is not associated with any selected channels.

Resolution

    To set the properties settings

  1. On the GUI toolbar, click the Login   icon and login with the 'admin' user account.  
     
  2. Click on the Setup () icon to enter the Setup menu.


     
  3. Click on Camera, The Camera menu appears.



     
  4. Click on Properties



     
  5. Left-click the Channel box, and select the channel to configure.  Lift-click / Right-click toggle up and down the menu.
     
  6. Click Audio box to select the audio channel.


     
  7. Associate the Audio input 1 thru 4 with the selected channel
     
  8. Click the X in the upper right corner to exit the Setup menu.
     
  9. Click OK to save the changes.