Default IP address of Spectra HD series

Issue

What is the default IP address of the Spectra HD series

Product Line

Pelco Cameras

Environment

Spectra HD series

Cause

Default IP address

Resolution

The default IP address of the Spectra HD series is 192.168.0.20 the camera will revert to this address if a DHCP server is not found.