Where can I get the spec sheet for the Endura workstation?

Issue

Where can I get the spec sheet for the Endura workstation?

Product Line

Pelco Video Management

Environment

  • Endura WS5050
  • Endura WS5060
  • Endura WS5070

Cause

Information from the workstation spec sheet is needed.

Resolution

The spec sheets for the workstation are available on Pelco.com. The WS5050 and WS5060 are obsolete, so the spec sheets will be found under Discontinued Video Management Downloads. The spec sheets can also be downloaded from the links below.

Spec sheets: