Can the Continuum default user password (ACC) be deleted?

Issue

The project specifications call for there to be no default administrator password in the BMS.  Can the ACC user in Continuum be deleted?

Product Line

Andover Continuum

Environment

  • ACC
  • Administrator password
  • Continuum
  • CyberStation
  • Permissions

Cause

The project specification calls for there to be no default administrator password in the BMS.

Resolution

The Continuum default Admin user (ACC) can be renamed and permissions can be removed. It cannot be deleted.