Does DX4000 series DVR feature a battery backup to save the date/time?

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Time is not saving on DX4000.

Product Line

Pelco Video Management

Environment

  • DX4000 series

Cause

  • Motherboard backup battery defective.

Resolution

Option 1: Replace the battery on the motherboard with Pelco part number ZSPDX4004012.

 

Option 2: The battery can be replaced in the field by purchasing one from a local electronics store. Battery specs are below: