Sarix series camera MAC ADDRESS location.

Issue

Where is the Sarix series camera MAC ADDRESS located.

Product Line

Pelco Cameras

Environment

All Sarix Series Cameras

Cause

Locating brand new Sarix IM series camera MAC ADDRESS

Resolution

PHYSICAL LOCATION (MAC)

New Sarix series camera MAC ADDRESS can be found within the kits bag of the shipping box. The MAC Address is also attached to the Sarix Camera via labeling.

 
WEB OR UTILITY (MAC)

Logging into the cameras IP Web Page will display the mac information.

  1. Click on Settings tab
  2. Click on the Network tab
  3. View "Hardware Address" for mac address.


The MAC Address may also be found by use of Pelco Device Utility 2/Endura Utility to scan for the cameras in the network. View of the Mac Address is displayed via the System Attributes tab-right view pane.

View here Lessons Learned Article LL#8397 for "Where to Download Endura Utility".

 

Note: For Multiple IP Camera installations, it is recommended to create a Log-Book of all IP cameras and attach one of the spare Mac Address labels as the identifier.