C20-DW-6 IR Sensitivity

Issue

What is the IR range for the C20-DW camera?

Product Line

Pelco Cameras

Environment

  • C20-DW-6

Cause

Require IR range for selection of IR light

Resolution

The C20-DW-6 camera IR Sensitivity range is 850nm >40% Peak Response.