When using Maxwell cameras at 3 megapixel the secondary stream must be set to H.264 to be viewed by Endura

Issue

Endura only uses H.264 when viewing megapixel streams., the secondary stream must be set to H.264 in order to be viewed

Product Line

Pelco Cameras, Pelco Video Management

Environment

Maxwell cameras in 3 megapixel secondary stream mode when being viewed by Endura

Cause

The Endura system uses H.264 to view megapixel streams, the camera must use H.264 to be viewed.

Resolution

Set the secondary stream to H.264 in order for it to be viewed by the Endura system.