Issue
When a trend log is opened up from Vista Workstation, there are no values or information in them. The trend logs are empty.
Environment
- Vista Workstation
- Trend Logs
Cause
The computer or user permissions do not allow Vista to create new directories.
Resolution
Check the $queues folder in the Vista database. If the $queues does not have the insertevents and insertlogvalues folders underneath it then create these folders manually. Now check the trend logs in Vista Workstation again, all of the trend logs should show up.