Schneider Electric SITESTAT

Issue

What is SiteStat and where can I find documentation on this product?

Is the SiteStat hardware supported by the Schneider Electric repair department?

Product Line

Andover Continuum, Other

Environment

SiteStat

Cause

SS-SCI controller has failed and a repair or replacement is needed.

Resolution

While the SiteStat product line is no sold or supported by Schneider Electric, a compatible replacement for the SS-SCI controller is the SS-NT-SSA16/CLK which is available on iPortal.

Information on SiteStat can be found here!